Technical FAQs

Ask a Question

What is the physical description of EM1000/EM1200 energy meter terminals located on the rear panel

  • 14 terminals are provided, seven terminals on each side
  • Six terminals for current, one in and one out per phase 
  • Four terminals for voltage, for three phases and neutral  
  • Two terminals for auxiliary power supply (control power)  
  • Two terminals for the POP (EM1000) or RS 485 communications port (EM1200)


Was this helpful?
What can we do to improve the information ?