Technical FAQs

Ask a Question

What are the possible system type field configurations are supported in EM1000 series energy meter

Supports the following configurations of System Type (field configurable): 
Direct 4-wire Wye (Star);
3-wire Wye (Star);
3-wire Delta;
2-phase 3-wire 
(2-phase); single-phase. 
Was this helpful?
What can we do to improve the information ?