Technical FAQs

Ask a Question

What is the correct function of GVAD0110 contact installed with GV2 MPCB

Please note that in the GVAD** contact block, the contact 95/96 reports trip condition only. 
GVAD** contact block is a fault condition contact only, this is why it is associated with normal contact to report in the same time the product status ON or OFF 
If you switch ON/OFF the GV2 the 95/96 contact will not change. This contact will change in case of trip only. 
The other contact 51/52 of GVAD** will be working fine with the ON/OFF button, for example if 51/52 is NO in OFF position then in ON position it will be closed (NC). 
Was this helpful?
What can we do to improve the information ?