Technical FAQs

Ask a Question

What is the cross reference of LC1D170**C ,250A Contactor.

LC1D-170** model contactor range is only manufactured for China and must be used only in the Chinese market.
Someone of your customer brought some machines or other parts from china and these contactors are installed in that machine. This range of contactor is not availablle on international pattern.

For taking all the technical details & specification, In replacement of this contactor refer the LC1F185** contactor which is available for international market. (** replaced by control voltage).
Also before referring it please check all the specification, dimension, mounting & type of application.
Was this helpful?
What can we do to improve the information ?