Technical FAQs

Ask a Question

What is the clearance and creepage distance between two main pole, auxiliary contacts in LC1D range of contactor.

Our product are complying to IEC60947-4-1 standard overvoltage category 3, pollution degree 3 for the clearance & creepage distance. So these are complying with the specification as mentioned in this IEC. 
Please refer the attached file having the details of clearance & creepage distance as per the voltage rating & impulse withstand voltage for LC1D range contactor.
Was this helpful?
What can we do to improve the information ?