Technical FAQs

Ask a Question

What is the painting thickness of Spacial SF universal enclosure (RAL 7035 grey).

The avergar thickness of this RAL 7035 color is 60 microns, the range could be in between of the 50-70 micron. It is only considered as the average value of paint thickness as 60 micron.
Was this helpful?
What can we do to improve the information ?