Technical FAQs

Ask a Question

Is it possible to mechanically interlock 3 Masterpact NW

The mechanical interlock cable type for 3 Masterpact NW is possible.

The functions available are:
> 2 + coupling sources.
> 2 + source alternative sources.
> 3 sources, a closed unit.

Warning: the mechanical interlock cable with 3 breakers Masperpact NT is not feasible.

Was this helpful?
What can we do to improve the information ?