Technical FAQs

Ask a Question

Is it possible to put an ammeter block (LV432655, LV432656, or LV432855 LV432856) on a compact NSX in addition vigi module block.

It is not possible on compact NSX 400/630, put an ammeter block (reference: LV432655, if LV432656 NSX 400 or LV432855 LV432856 or if NSX 630) in addition to the Vigi module. 

Was this helpful?
What can we do to improve the information ?