Technical FAQs

Ask a Question

What are the class of accuracy Micrologic 5/6 E installed on the Compact NSX range for measuring parameters

Precision measurements of Micrologic 5/6 E installed on the range Compact NSX :

> Current: Class 1 according to IEC 61557-12,
> Voltage: 0.5%
> Power and energy: class 2 according to IEC 61557-12,
> Frequency: 0.1%.
Was this helpful?
What can we do to improve the information ?