Technical FAQs

Ask a Question

Is it possible to use same external power supply 24 VDC (AD module) for the power trip unit Micrologic Masterpact NT / NW and communication bus.

It is not recommended to use same power supply as the communication bus requires its own power supply 24 V DC (E1, E2), which is organized independently from the power supply 24 VDC  Micrologic (F1-, F2 +).
Was this helpful?
What can we do to improve the information ?