Technical FAQs

Ask a Question

if power supply ABL1 range has surge protection.

These ABL1 range of the power supply will have Surge Protection feature as per the IEC 61000-4-5 standards. This IEC 61000-4-5 standard will guide us the
compatibility with Lightning and industrial surges of the device.
For the ABL1 range , about Surge (IEC61000-4-5) , below are the details :

(Surge immunity test) 

On primary side :+/-1KV Line to Line ,+/-2KV Line to earth 

On secondary : +/-0.5KV line to Line ,+/-0.5KV Line to Earth 


Was this helpful?
What can we do to improve the information ?