Technical FAQs

Ask a Question

We are  having issue regarding web deployment, any changes made in SCADA at server is not reflected at web client screen . during complinig the new project , some warning and message "Failed to create web deployment files" shows.

There is an issue in Vijeo Citect v7.20, where the parameter [WebServer]deployRoot does not recognise as a valid value a path enclosed in double quotes. 
As a workaround, please use an access path without spaces in it, and do not enclose it in double quotes. e.g. [WebServer]DeployRoot=C:\temp\deploy.
or install the latest service pack 4 as this issue has been fixed in service pack.
 
Was this helpful?
What can we do to improve the information ?