Technical FAQs

Ask a Question

While upgrading the Vijeo Citect v7.0 project to our latest Vijeo Citect version 7.4 it seems that graphic pages are not upgraded successfully. My super genie updates and changes are not propagated out to pages with the genie on it., what may be the cause of the issue.

Make sure Fast Update Pages is off (under Graphics Builder, menu Tools, select Options), then update your pages in Graphics Builder.
If this does not work, then you need to create a new instance of the genie as per the steps below :
 
1. Change your super genies as desired.
 
2. In graphics builder, click the "Open" button at the top of the page. Select page tab. Delete the system page associated with the super
genie, ie a page with a name like "!mysupergenie". Note: this does not delete the super genie itself.

3. Click new page. Paste the genies onto the new page for each page deleted at step 2. Close, but don't save the page. If you click open
again, you'll see a new page created for each super genie.

4. Recompile, and start the project.


 

Was this helpful?
What can we do to improve the information ?