Technical FAQs

Ask a Question

We are unable to create, edit/delete and change password at runtime by using in built functions like create user, delete user, and password change. These function is not working until unless we shutdown and restart the runtime. What may be the cause of the issue.

This issue may occurs if an alarm server is not defined in your project. An alarm server is needed to update running system when using creating/modification functions such as UserCreate().
Define an alarm server in your project and you should be able to create and use new Citect users without restarting Citect.
Still if the problem occurs then make sure that you have not used any RDB functions like RdbOpen() or RdbClose() in your cicodes, which occupies the real-time database all the time, so the
new creating/change/deletion of user cannot be flushed into read-time database.
Was this helpful?
What can we do to improve the information ?