Technical FAQs

Ask a Question

Which PM800 series meter models has the Energy-Per-Shift feature

PM820 or above has the Energy-Per-Shift feature.
The energy-per-shift feature allows the power meter to group energy usage based on three groups: 1st shift, 2nd shift, and 3rd shift.
These groups provide a quick, historical view of energy usage and energy cost during each shift. All data is stored in nonvolatile memory.
Was this helpful?
What can we do to improve the information ?