Technical FAQs

Ask a Question

What communications ports are available on a PM800 series meter and when should each be used

Below are the Communications ports available in PM800 series meter's;
1. The PM800 series meter base unit has a 2-wire RS-485 port (Comm 1).
2. The PM800 Remote Display Module has a 4-wire RS-485 port (Comm 2).
3. The PM800 Ethernet Communications Card (ECC) has a 4-wire RS-485 port (Comm 3).

When should each port be used;
1. The base unit 2-wire RS-485 port should be used to communicate directly with a PM800 if you have a 2-wire RS-485 daisy chain.
2. If you have a PM800 with a Remote Display module (4-wire RS-485) and you have a 4-wire RS-485 daisy chain, use this communications port, if you have a 2-wire daisy chain use the port on the base unit.
3. If you have a PM800 with an ECC and you intend to use the ECC card as a gateway, you will need to connect the downstream RS-485 wiring to the port on the ECC card. This port is configurable for 2-wire or 4-wire via dip switches. If you connect downstream devices to another port you will not be able to access them via the ECC.
 
a. Note: If you have a Remote Display module and an ECC connected to the PM800 base unit, the communications port on the Remote Display module is not functional.
 
 
Was this helpful?
What can we do to improve the information ?