Technical FAQs

Ask a Question

Is the configuration of an Ethernet communication module ECC card stored in the meter or in the card itself

The configuration of the ECC (IP address, subnet mask, default gateway) is stored in the meter itself. If an existing meter with an ECC is replaced but still uses the original ethernet card, then the configuration will have to be set again in the new meter.

Was this helpful?
What can we do to improve the information ?