Technical FAQs

Ask a Question

Can we change the Modbus TCP/IP equipment Unit ID from the HMI Target

For changing the Unit ID, go to Configuration Menu of the HMI target and select "Offline" tab. In this tab, you see "I/O Manager". Here you will see Driver Configuration Button and Equipment Configuration Button. Press the Equipment Configuration button to change the Unit ID. Additionally you can also create a switch in Vijeo designer and set the operation to "System" and select the "Configuration" option. You can not change the Unit ID using some script in vijeo designer.
Was this helpful?
What can we do to improve the information ?