Technical FAQs

Ask a Question

Is it ok to connect only one of power supply V-,V+ of A and B connection on ACE949-2 for use data line of A and B?

ACE949-2 communication interface is used for 2-wire RS-485 communication and the serial ports A and B are used for daisy chain connectivity. 
So if it is using with the other sepam relays then you have to take all the terminals A & B for the wiring means all connection of power supply on all ports has to be done.
 
Refer the attached sheet for the connections and other details.
Was this helpful?
What can we do to improve the information ?