Technical FAQs

Ask a Question

What are the Acti9 range meter models with pulse output are compatible with the Acti9 Smartlink

Schneider Electric energy meters as per the below listed references with pulse output are compatible with the Acti 9 Smartlink; 
****** Direct measurement (up to 63 A) 
1. iEM3110 (the pulse weight can be configured) 
2. iEM3155 (the pulse weight can be configured) 
 
*****CTs inputs (1 A, 5A) 
3. iEM3210 (the pulse weight can be configured) 
4. iEM3255 (the pulse weight can be configured) 
 

Was this helpful?
What can we do to improve the information ?