Technical FAQs

Ask a Question

How Acti9 Smartlink calculates the energy consumption and average power based from pulse input.

Acti 9 Smartlink calculates the energy consumption and the average power between 2 pulses. 
 
Energy consumption = Number of pulses counted × pulse weight 
 
Average power between 2 pulses = (3600 × Pulse weight)/t; the result is expressed for one hour. 
Was this helpful?
What can we do to improve the information ?