Technical FAQs

Ask a Question

What are the technical details of RJ45 cable is used for Modbus communication with compact NSX range of MCCB.

This RJ45 cable is a straight connection cable. This is a shielded cable with 4 twisted pairs of mini 0,15mm² (AWG26), of characteristic impedance 120 ohms.
Please find out the pin connection of this cable coneector in the attached file.
Was this helpful?
What can we do to improve the information ?