Technical FAQs

Ask a Question

Can we use Acti9 Smartlink digital output for direct controlling of the devices

Acti9 Smartlink Output maximum current is 100mA/24V DC.
Devices consuming less than 100mA can be connected directly to digital output of Acti9 Smartlink

Example:
Was this helpful?
What can we do to improve the information ?