Technical FAQs

Ask a Question

Is it possible to use Acti9 MCB iC60N/H/L at DC network.

Yes, It is possible to use the iC60 range of MCB on DC network as the specification given in the catalog. Please refer the attached declaration for showing the same specification.
Was this helpful?
What can we do to improve the information ?