Technical FAQs

Ask a Question

What are the technical details of DK1JC23 and what is the standard cross reference of DK1-JC23 reference

The DK1JC23 was a 3 poles fuses switch disconnector size 1 fuse rated for 315A maximum. Please refer the attached available catalog page for the technical specification of DK1JC23 
Today it can be replace by GS2QQ* fuse switch disconnector range from available offer. You will have to be aware the the fuse in GS2QQ will size 2. 
Was this helpful?
What can we do to improve the information ?