Technical FAQs

Ask a Question

What is the IP protection degree of RM6 panel, Is it IP 31 or above.

The IP degree of protection of RM6 units is globally IP2X (internal between cable boxes) and IP3X on front face. 
Was this helpful?
What can we do to improve the information ?