Technical FAQs

Ask a Question

What is ALE011 error on Lexium 23D drive.

ALE 011 is the Encoder Error. It might possible that the wiring of the encoder is in correct,
Please re-check the wiring of encoder.
It is recommended to use the shielded twisted- pair cable. Refer to attached document.
Was this helpful?
What can we do to improve the information ?