Technical FAQs

Ask a Question

Can I connect & access Profibus PA devices using PRM module

To connect PA devices you must use a DP/PA converter.  Once Profibus PA device is linked to the PRM device, Unity pro can be used to manage diagnostics and calibration of  instruments using the Device DTM, or from any other FDT compliant tool, using the COMM DTM service.
Was this helpful?
What can we do to improve the information ?