Technical FAQs

Ask a Question

What is the difference between ramp stop and freewheel stop on Altivar71/61 drive.

Ramp stop:- 
Motor stops via ramp [depending on DEC time - Time to decelerate from the [Rated motor freq.] (FrS) to 0. ]

Freewheel stop:-
Motor stops by its own inertia, not via ramp.
 

Was this helpful?
What can we do to improve the information ?