Technical FAQs

Ask a Question

Is there any instructional manual available for Thermal control Electronic hygrotherm NSYCCOHYT230VID.

The NSYCCOHYT230VID is an electronic temperature and humidity controller.

Features:

● Input voltage: 220-240 V.
● Hygrotherm with 2 independent switching relays (ventilation / heating function).
● Thermostat precision: +/–1.5 °C.
● Hygrostat precision: +/–5% RH, relative humidity.
● Option of installing external PTC sensors, ref. NSYCCAST, for remote reading (L = 3 m).
● PC plastic material, self-extinguishing according to standard UL94 V0.
● Option of displaying the temperature in degrees Celsius °C or Fahrenheit °F.
● Operating temperature 0 °C…+50 °C
● Temperature setting range +5 °C…+50 °C
● Humidity setting range 20%…80%
● RH hysteresis 3%


Please refer the below attached instructional manual.

Was this helpful?
What can we do to improve the information ?