Technical FAQs

Ask a Question

Is there any instructional manual available for Thermal control Electronic hygrostat NSYCCOHY230VID.

The NSYCCOHY230VID is an electronic humidity controller.


● Input voltages: 110-240 V.
● Precision: +/- 5% RH, relative humidity.
● Hygrostat with 2 independent switching relays (ventilation / heating function).
● PC plastic material, self-extinguishing according to standard UL94 V0.
● 2 operating modes for RH %: relative humidity control and dew point control.
● Humidity setting range 20%…80%
● RH hysteresis 3%
● Internal sensor element Internal humidity sensor

Please refer the below attached instructional manual.

Was this helpful?
What can we do to improve the information ?