Technical FAQs

Ask a Question

Is it possible to padlock EasyPact CVS 100...630A circuit breaker when equipped with a direct/extended rotary handle.

Yes, it possible to padlock EasyPact CVS 100...630A circuit breaker when equipped with a direct/extended rotary handle.
 
Direct rotary handle - standard situation, in the OFF position, using 1 to 3 padlocks.
 
Extended rotary handle - Padlocking locks the circuit-breaker handle and disables door opening.
                                             standard situation, in the OFF position, using 1 to 3 padlocks.
 
Was this helpful?
What can we do to improve the information ?