Technical FAQs

Ask a Question

Is there any way to write the tag values in VJC runtime without login the username.

With the introduction of enhance security measures in V7.10 a user must be logged in before tags can be written to. Therefore a user must be create in the project and logged in before any means of writing to tags be performed (Cicode, reports etc.). 

Alternatively this behavior can be changed by changing editing the [LAN]SecureLogin = 0 citect.ini parameters but a full understanding of the implications must be acknowledged before doing so.  

Was this helpful?
What can we do to improve the information ?