Technical FAQs

Ask a Question

After up gradation of Vijeco Citect project from V 7.1 to V 7.3 we are facing problem during compilation of project. It is showing errors “Storage Method is not defined” in the trends configurations.

The project backup`s that was configured with older versions like of Vijeo Citect V7.10 or V7.00, when you try to restore this project on the Vijeo Citect V7.30 then it gives you compilation error messages for the "Storage method" in the trend tags as in Vijeo Citect previous version it is not mandatory to set the Storage Method like 2 Byte or 8 Byte in the trends tag configuration.
So you have to modified this in your project inside Trends Tag configurations and after changing this the project will compile successfully .
Was this helpful?
What can we do to improve the information ?