Technical FAQs

Ask a Question

What is the service life of the Acti 9 ARA automatic recloser.

The sevice life of Acti 9 ARA automatic recloser is given in terms of mechanical and electrical endurance is given below
> The mechanical endurance of the ARA + iC60 combination is 10,000 switching cycles (O-C), and for the ARA + iID
  combination is 5,000 switching cycles (O-C).
> The electrical endurance varies depending on the use of the circuit breaker or the associated residual current circuit breaker
  (rating, derating, class of use, pf).
Was this helpful?
What can we do to improve the information ?