Technical FAQs

Ask a Question

Historian Web Client cannot display published information with error "Unexpected error (0x8003001e) [Microsoft ADO/RDS]" on Windows 7 SP1 or Windows Server 2008 R2 SP1 machines.

After successfully logging into the Historian web client and clicking on the Web Client button, the web client displays the following message: Unexpected error (0x8003001e) [Microsoft ADO/RDS]. 
The cause of this issue is due to Microsoft security update KB2698365 that blocks the Historian web client. This is caused by a broken binary compatibility between msado15.dll v6.1.7601.17514 (the original) and v6.1.7601.17857 (KB2698365). Therefore, the incompatibility occurs in RDS components at the time when a recordset is marshalled back to Historian web client. The error code 80004002 in IIS log means "No such interface supported".
For further information about KB2698365 and the issue it addresses refer to http://technet.microsoft.com/en-us/security/Bulletin/MS12-045.
 
Microsoft KB2734642, "RDS-based applications crash in Windows 7 SP1 or Windows Server 2008 R2 SP1" resolves problems related to KB2698365 (MS12-045). It installs a new msadcs.dll v6.1.7601.17912. Customers who experience error 0x8003001e after installing KB2698365 are advised to install KB2734642(http://support.microsoft.com/kb/2734642) in their environment.
Was this helpful?
What can we do to improve the information ?