Technical FAQs

Ask a Question

Can Acti 9 atomatic recloser ARA be combined with a 1P, 2P, 3P or 4P circuit breaker.

The automatic recloser ARA is available in four versions: ARA iC60 and ARA iID, 1P/2P and 3P/4P. It can be combined with all the iC60 1P,
2P, 3P and 4P circuit breakers and iID 2P and 4P residual current circuit breakers of the Acti9 range:
Was this helpful?
What can we do to improve the information ?