Technical FAQs

Ask a Question

Can we use Web Clients on Static license or it will have a Floating license only . How to consider Web client points, is it based on Server IO points or can i take it as per requirement . 

You can`t use a static license for the Web Client as the web client will always check for the license on the IO Server`s key.
If you want to use the web clients then the number of points on server & client will remains same & in case if you are using a normal Citect client then a separate static license can be used and in that you can take the different point counts from Server license.
Was this helpful?
What can we do to improve the information ?