Technical FAQs

Ask a Question

What is the reference single mode fiber optic cable that is used to connect the Ethernet port processors Quantum 67261

140CPU67261 Quantum CPU's has one Ethernet port used as a Hot Standby port. The reference fiber optic cable used for connection is VDIF0646463505.  This is an optical type 5 meters long  9/125 microns single mode cable with LC type connectors.
Was this helpful?
What can we do to improve the information ?