Technical FAQs

Ask a Question

Can we compare two Unity pro applications imported from different versions.

Unity DIF v8.0  is an comparison software that compares two Unity Pro project files and represents the differences graphically with the similar look and feel of Unity Pro. This enables the user to understand the project differences easily. Unity DIF can compare and provide differences for the following sections of Unity Pro project files:
·         PLC Configuration (Hardware and Network)
·         Derived Data Types
·         Derived FB Types
·         Variables and FB Instance
·         Motion
·         Communication
·         Programs
·         Animation Table
·         Operator Screen
·         DTM Catalogue
Unity DIF 8.0 software can compare .sta, .stu, .zef, and .xef project files of Unity Pro
Was this helpful?
What can we do to improve the information ?