Technical FAQs

Ask a Question

How to configure Ethway Protocol in a Windows XP PC.

Open Local Area Connection from My Network Places. Right click go to "Properties" tab. Then click on the "Install" . In the next window Select "Protocol" option and then press "Add" Tab.
After pressing Add, new popup window opens where you have to click on Have Disk. Here Provide the Path for the Ethway driver setup file. After Completion of setup Ethway protocol will be visible in connections.



Was this helpful?
What can we do to improve the information ?