Technical FAQs

Ask a Question

How to configure an extension rack using M340 BMXXBE1000 module

M340 supports configuration of multiracks. The address of each rack is determined by the position of the micro-switches on the unit BMXXBE1000.
Rack address depending on the position of the switches is given in following table:
Was this helpful?
What can we do to improve the information ?