Technical FAQs

Ask a Question

In Concept can we define variable names starting with numbers

According to the standard IEC 61131-3 , the first character of the variable name must contain only letters. If however, you want to use numbers as the first character of a variable name,  you can go to the menu " Options " " Environment " IEC Extensions "and check the" leading figures qualifier allowed “.

Was this helpful?
What can we do to improve the information ?