Technical FAQs

Ask a Question

How can i read the clock of a NTP server using Unity Pro

To read the clock of a NTP server from the application controller, use the R_NTPC function in the fast main task or interruption.
The R_NTPC function is available for M340, Premium and Quantum PLCs. It is used to recover the date and time for an NTP server in two formats:
  • A display format.
  • A calculation format.
NOTE: This function requires connection to an Ethernet network enabling access to an NTP server. 
 
Was this helpful?
What can we do to improve the information ?