Technical FAQs

Ask a Question

What is maximum explicit massaging size for a 140NOC78100 module

140NOC78100 supports Explicit massaging on both EtherNet/IP & Modbus TCP. On EtherNet/IP maximum messaging size is 1023 Bytes however on Modbus TCP maximum message size is 250 bytes READ & 240 bytes WRITE.
Was this helpful?
What can we do to improve the information ?