Technical FAQs

Ask a Question

What is the derating factor for the AFE (Active Front End)  to be used with Altivar 71/61.

There is no derating factor for the AFE (Active Front End), but due to the required derating of the Altivar 71/61 drive the allocated AFE is automatically derated.

Was this helpful?
What can we do to improve the information ?