Technical FAQs

Ask a Question

In Quantum ERIO which module supports Scada connection at 1GBps transmission speed

140 NOC78100 has four ports out of which two ports are meant for control network. These two ports can be configured with Scada for 1gbps connection.
A Control Network is a Ethernet-based network containing PLCs, SCADA systems, an NTP server, PCs, AMS, switches, etc. Two kinds of topologies are supported:
  • flat — Devices in this network belong to the same subnet.
  • 2 levels — The network is split into an operation network and an inter-controller network. These 2 networks can be physically independent, but are generally linked by a routing device.
Was this helpful?
What can we do to improve the information ?