Technical FAQs

Ask a Question

What are the types of mounting system for Acti9 Smartlink.

The two mounting types are for Acti9 Smartlink:

1. With Multiclip 80 or 200 which allows control and power cabling totally pre-fabricated.

2. Without Multiclip, using dedicated accessories (mounting kit), which allows mounting in existing panels.

Was this helpful?
What can we do to improve the information ?