Technical FAQs

Ask a Question

What would be the maximum consumption of Acti9 Smartlink with Acti9 devices connected and Third party devices are connected.

Assuming that all I/O are used:
 
> Smartlink maximum consumption 35mA
 
> Device from Acti 9 range :
Consumption input= Consumption output = 5 mA
Maximum consumption = 35+[ (3x5 mA) x 11 channels] = 200 mA
 
> Third party devices
Consumption input= 5 mA 
Consumption output = 100 mA
Maximum consumption= 35 +[(2 x 5 mA)+100mA] x 11 channels= 1,3 A

Was this helpful?
What can we do to improve the information ?