Technical FAQs

Ask a Question

How can i read all the position status of Acti9 Smartlink (from channel 1 to channel 11) at once (with only one request).

On 120 register address you can read all  the position status of Acti9 Smartlink (from channel 1 to channel 11) at once (with only one request).
Refer attached "Address Zone Table"
Was this helpful?
What can we do to improve the information ?